AXIS#.OBS.ENABLE

Description

AXIS#.OBS.ENABLE turns the Observer on and off. When the Observer is in the disabled state (0), it passes the raw velocity feedback into the control loops.


  • This setting cannot be changed while the amplifier is enabled in order to minimize unexpected disturbances.

The Observer is made up of a few components. Following is a block diagram of how the Observer is connected in the loops.

Versions

Action Version Notes
Implemented 02-04-03-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 1
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
AXIS1.OBS.ENABLE

5017h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.OBS.ENABLE

5117h

02h

Unsigned8

-

-

Read/Write

No